Other Parts Discussed in Thread: CC2591
Hi,
Following the thread in https://e2e.ti.com/support/wireless_connectivity/zigbee_6lowpan_802-15-4_mac/f/158/t/617328
As mentioned in the above link, there is an issue with the range between router to router. We have done the output power analysis, with Power amplifier (CC2591), output power is 15dB, and without Power amplifier output power is 0.5dB which is measured using spectrum analyzer. But the range is similar in each cases. Is any further modification should be done in schematics to achieve longer range with power amplifier(cc2591).