This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538DK: Receiver test with Zigbee Equipment R&S CMW100

Part Number: CC2538DK

Hello,

Our custmer is testing CC2538DK with Zigbee Equipment R&S CMW100.

https://www.rohde-schwarz.com/us/product/cmw100-productstartpage_63493-143617.html

But, They can't receiver test on CC2538DK with CMW100.

How can test receiver test with Zigbee Equipment CMW100?

* Wavefrom on CMW100

LRWPAN_2450MHz_OQPSK_127Bytes_PRBS9.wv
This waveform is generated using a Matlab Model. Configuration information is as follows;
Parameter                           Value
PHY                                     2450MHz OQPSK
Nof Payload Bytes              127 (including 2 CRC bytes)
Payload Pattern                   PRBS9
Waveform duration              5ms