device sends mac data req continuously
then it send orphan notification in packet no.- 38097,
rejoin request in packet no.-38130
rejoin response with association successful in packet -38251,38254
then why ZNP send leave in packet -38271,38288
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
device sends mac data req continuously
then it send orphan notification in packet no.- 38097,
rejoin request in packet no.-38130
rejoin response with association successful in packet -38251,38254
then why ZNP send leave in packet -38271,38288
data req orphan rejoin req rejoin resp leave.rar
z-stack 3.0 for ZNP and ZR (cc2538-cc2592emk)
Z-stack 1.2.2a for ZED (cc2650)
1) Having just received a rejoin request the ZR/ZC would expect an acknowledgement of the rejoin response from the ZED, similar to other Zigbee packet transactions. Upon not receiving one the routing device assumes an error was made and sends a leave request to clean up the association.
2) You will need to provide a log of this behavior, if a parent device is polled by an end device which is not its child (due to being expired or not being its child at all) then the parent device must request this end device to leave the network with rejoin set to TRUE so that this device can rejoin the network and find a new parent (which could be the same router or another one). Device and parent announcements help routing devices determine if their children have been picked up by other parents or not.
3) My mistake, I was confusing it with Pan ID 0x0F7C.
Edit: Thread closed unless more information is provided.
Regards,
Ryan