Hi,
I am using CC2530 home stack using Z tool.
I am facing issue when I set the channel or PANID.
When my device set as coordinator, and I suppose to make changes in its Channel or PANID i am unable to change both,
But when I reset it factory defuatlt then I can make it both.
I am following below process to make it , kindly verify below process are right or I am doinf something wrong;
Step 1) SYS_OSAL_NV_Write
ID 03
Offset 00
Len 01
VAlue 03
Step 2) Hard reset the device.
Then I chaneges the both value using
1) UTIL_SET_PANID
2) UTIL_SET_CHANNEL
then hard reset the device after hard reset I will perform ZB_Start_request
Then my paniid and channel ID refelcts,
but at this time I need to change both value suppose I want one of the previous value ( from PANID , Channel ) then what i need to do....
Please suggest your suggestion