EV2300 drivers for 64-bit Windows

These alternative drivers for the EV2300 are provided as a courtesy and are not officially supported by TI.  They should enable a 64-bit Windows system to work with EV2300, but are provided as-is.  For official support with using gas gauge evaluation software and tools on a 64-bit Windows system, please use the EV2400 module.

Also note that some older bqEVSW will require the installation of the support components contained in SLUC291.  Use of newer GUIs like GaugeStudio or Battery Management Studio do not require the installation of the support components.

For use of bqEVSW with EV2300, here are the recommended steps:

  1. Install unofficial 64-bit drivers for EV2300 from the zip archive attached to this post.
  2. Install the desired bqEVSW package from the corresponding gauge product folder on TI.com.
  3. Install the support components from this link: http://www.ti.com/lit/zip/sluc291

NOTE: "Install" means to right-click on the .exe file and select "Run as administrator", then select "Yes" from the pop-up window and run the installer.

Anonymous
  • 您好:

       我是北京世纪东方的,正在使用贵公司的bq20z75芯片及相应软件,过程中遇到以下几个问题,希望您能帮我解决一下。

    1、 对于芯片bq20z75-v160与bq20z75-v180,是否均支持sluc135新增的电芯品牌特性的电芯规格?

    2、 设置chemistry ID,是否可以只修改“chem. ID ”为0135,还是必须在“bqeasy”中,配置化学特性为0135?

    3、 电池在充放电过程中,容量不稳定, 导致问题出现的原因可能是什么?