Part Number: ISO1412DWEVM
Other Parts Discussed in Thread: ISO1412
Hello,
in the schematics J7 connector, 2 & 4 pins are GND but 1 & 3 mentioned as GND. Can you check this.
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO1412DWEVM
Other Parts Discussed in Thread: ISO1412
Hello,
in the schematics J7 connector, 2 & 4 pins are GND but 1 & 3 mentioned as GND. Can you check this.
Regards, Holger
Hi Holger,
Thanks for reporting this discrepancy and mismatch between schematic and PCB layout.
The actual PCB has J7 pin1 connected to Z and pin 3 connected to Y of ISO1412 while pins 2 and 4 are connected to GND2 of ISO1412. I also agree that pin Z is incorrectly referred as P and Y as N, a correct labeling would consider Y to be P and Z to be N. I will look into these issues and mismatches and correct them accordingly.
Thanks again for reporting this to us. Let me know if you have any further questions, thanks.
Regards,
Koteshwar Rao