Other Parts Discussed in Thread: ASH, TPS2420
Hi all,
Just finished the assembly of a few prototype boards and have encountered the following issue. While the circuit correctly outputs 7.4V ±0.1V while not under load, when a 0.6A load is applied the output voltage from the LM2679 drops to around 6V.
Fortunately though the 6V output will still work for our application but we would like to sort this issue out.
Attached below are the schematic, board layout, components and images from a scope reading the output voltage.
Component Values:
IC: LM2679SD-ADJNOPB
Cboost: 10nF
CSS: 10nF
CIN: 2X 56uF
COUT: 2X 47uF
RFB1: 1K
RFB2: 5.11K
RLIM1: 5.9K
Inductor: 22uH 60mOhm



Any help would be greatly appreciated as we are looking to get these boards into production soon, Thanks!
Ash