Other Parts Discussed in Thread: LM5575, LM61440, LMR16010, LMR16020
Hi,
Our project needs to convert +18V -> +10V and -18V -> -5V, each 100mA current max, switching frequency > 400kHz, both branches synchronized to avoid interferences. Spread spectrum would be a bonus :-) Please is there any option from the TI selection? I found an older AN https://www.ti.com/lit/an/slyt516/slyt516.pdf and a design https://www.ti.com/tool/PMP9624 but the synchronization requirement complicates it. The device will need other DC/DC converters for +24V -> +18V, an invertor to -18V, would perhaps some central power manager with multiple outputs capable of positive and negative voltages, with one common frequency be available, with external mosfets for the respective outputs?
Thank you very much for any help and suggestions.
With regards,
Pavel.