Part Number: TMS320F280023C
Other Parts Discussed in Thread: C2000WARE-MOTORCONTROL-SDK, C2000WARE
Hi,
I am using TMS320F280023C to run BLDC motor using Trapezoidal control. For the same hardware, I had run a BLDC motor rated 48V , 750 W, 24 pairs pole. Now I have changed to 48V, 1.2kW, 4 pole pairs BLDC motor. But after changing to new motor, it takes lot of current with very low duty as well. There is lot of vibration, and due to high current motor is not running for more than a minute ( that too duty < 20%).
Note : Resistance and Inductance of new motor are 1/4th time of old motor. and PWM frequency used here is 16kHz.
Could you please suggest, why is that happening with new motor?