This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430: Fluctuation in voltage even at low current

Part Number: TPS5430


Input regulated 24VCC

Output 12V 3A

Components values calculated at WEBENCH® Power Designer

Voltage 12v drops to 11.45 at 89mA

Attached schematics and pcb layout both taken from datasheet

Copper pour now shown but applied to pcb.

Ripple is at an acceptable level and overall the circuit is working fine but my client is asking me for a better solution.

Thanks for your help.

Marco