Part Number: TPS2378
Hello
I use TPS2378 on our product, I measured output voltage at TPS2378 (between VDD and RTN pins) and inrush current between PSE (PoE injector) and our device. The ramp up time of the output voltage is very fast, I've measured typically 25 to 30us, see picture below (red line is PoE output voltage, orange is inrush current, ignore blue line). I have a PoE injector with 55V output voltage. There are 4x 2u2 capacitors at the output, so I = 8.8u * 55 / 27u = 18A, I measured about 20A inrush so it corresponds to the capacitors. TPS2378 datasheet says it has "140-mA inrush current limiting", so it is not clear to me why the limiting is not working. I have TPS2378EVM-105 board and I measured same fast ramp and high inrush current on this board too. Do you know why the ramp up and the inrush current is so high? Can I fix it somehow and limit the inrush current?
Thanks a lot
Best regards
Libor