Part Number: LM3940
Other Parts Discussed in Thread: TMP302, TLV755P
I have a few questions about a design I'm creating using the LM3940 voltage regulator to power the TMP302 temperature switch.
The first question is very straightforward. For the exact model of the LM3940, I'm deciding between the LM3940IMP-3.3/NOPBCT-ND and the LM3940IMPX-3.3/NOPBCT-ND models. I can't find any difference between the two, so if there isn't any I would just use the cheaper option.
The next question is similar to the other questions asked about the LM3940. I've attached the schematic for the circuit I'm making for reference. I see other people saying not being in the ESR will lead to instability, but all of those questions seemed like they were receiving a noisy supply power. I'm getting my voltage from the 5V line of a USB, which I expect to be far less noisy. If I use ceramic capacitors, will I run into the same problem with instability?
Lastly, I didn't use a copper pour on my PCB to dissipate heat from the regulator since I didn't want that to interfere with the operation of the temperature switch. Do you think the voltage regulator will still properly be thermally regulated without it?
Thank you in advance.
-Sean