Other Parts Discussed in Thread: TPS7H2201-SP,
Hi,
- Pin 1-4: 4.90V
- Pin 5: 0V
- Pin 6: 0.66V
- Pin 7: 0.4V
- Pin 9: 0V
- Pin 10: 0V
- Pin 11: 0V
- Pin 12: 0V
- Pin 13-16: 0.4V

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,

Hi Marcel,
After doing a sanity check, I don't see anything wrong with the schematic in your post. I do have a couple questions to help figure out steps to move forward.
Before sending back any possibly defective units for failure analysis, it is recommended to perform an "A-B-A" swap of the part onto a known good board. This will confirm whether the part, or board is causing the issue. A full description of the process, as well as other guidelines for the return process can be found on page 2 SPRAC01A.
After performing the "A-B-A" swap, if the device is non-functional, a customer product return can be requested here. Make sure to select the "Failure Analysis" option to request a failure analysis.
Hi Andy,
1. Yes that is the case, it's been running since January 2023
2. Yes, same schematic and they are functioning properly
3. It was not
4. Sorry for the confusing, using the TPS7H2201-SP. Specifically this was the TPS7H2201HKR/EM that isn't working.
Can be swap a new part onto the same board instead of the A-B-A swap?
Hi Marcel,
Yes, swapping a new part onto the same board will work to verify that the board isn't causing an issue.
If the new part works with no issues, go ahead and submit the customer product return with a request for failure analysis.
When removing the part from the board, ensure it is done carefully so that the part is not damaged in the removal process.
Let me know the result of the swap and when you submit the product return, or if you have any additional questions or issues.
Thank you,
Andy Fondaw
Hi Andy,
Sounds good, thank you. Is it possible for TI to send a replacement TPS7H2201HKR/EM part? I submitted a sample request yesterday.
Hi Marcel,
After the device has been returned to TI, if the failure is confirmed to be due to nonconforming device, TI may offer replacement or credit at that time.
Regarding your sample request, unfortunately TI does not broadly offer free samples for space products, but your request will be reviewed by our business team.
Apologies for any inconvenience,
Andy Fondaw
Hi Andy,
We replaced the part with a new one and the system works. Can you send a label for us to ship the nonconforming part?
Best,
Marcel
Hi Marcel,
I'm glad to hear your system is working with a new device installed.
Please use the TI customer returns page (linked here) and fill out the form to initiate the return process. Please make sure to select "Failure analysis" so we can confirm a nonconforming device.
Thanks,
Andy Fondaw
Marcel,
Please continue to follow the customer return process for failure analysis on this device.
I will close this thread now, but you can still respond to re-open it if needed.
Thank You,
Andy Fondaw