It's the first time I deal with a PoE Design. I decided to use the TPS23755 for my first design and as I continue drawing the circuit and selection the required components, unfortunately I have to realize that I do not have access to samples for the PoE transformer from LinkCom "LDT0950-50" used in the design.
I tried to find a replacement part but the two parts I found do not have exactly the same specifications.
-) Wuerth Electronics: Part number: 7491199112
-) Coilcraft; POE13P-12L
The parameters for the inductance value differs - 127µH instead of 150µH
and
Turn Ratio is also different 2:1:1 instead of 2.25 and 2.57.
What I can say is that it is not required for my design that the output voltage is exactly 12V. It is allowed for the design that the output voltage is in the range of 9V to 14V. However I do not the effect the different turns ratio applicable to the auxiliary winding used to supply the TPS23755.
Can you give me some hints what I can do using the TPS23755 and having no access to your transformer from the reference design?
I hope you can help me.
Best regards
Johann Teufelhart