Other Parts Discussed in Thread: TPS3700, INA2180
I am using the TPS63700 to generate a negative supply in a manner that relies on an external, variable reference instead of the reference provided by the VREF pin of the TPS63700. My reference's adjustment range is 0 V to +1.8 V. Interestingly, when my reference is at 1 V or less, the output of the TPS63700 tracks accordingly and its voltage agrees with equation 1 on page 13 of the datasheet. The feedback voltage is also at the correct value of 0 V when my reference is 1 V or less.
Once I increase my reference above 1 V, I see the feedback voltage begin to increase and the output of the TPS3700 remains at a fixed voltage, regardless of the value of the reference voltage above 1 V. I have attached a screenshot of my schematic for reference.