Part Number: BQ25185EVM
Other Parts Discussed in Thread: BQ25155, BQ25185, BQ25180
Tool/software:
Hi everyone,
I’m in need of a battery charger IC for a project where I need to charge a Li-ion battery (3.7-4.2V) using either another Li-ion battery (3.7-4.2V, typically close to full charge) or a USB source (5V).
I’ve encountered an issue with the BQ25185EVM where the charging process halts if the voltage difference between the input (Vin) and the battery (Vbat) is less than 300mV. For example, when Vin is 4.1V and Vbat is 3.9V, the charger does not start and enters sleep mode.
Can anyone suggest a suitable charger IC that can handle this scenario? I am open to both standalone RC-controlled or I2C-controlled options.
Thank you for your help!