This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650331-Q1: Will need to look for the PMIC to support LP5 (PMIC5200)

Part Number: TPS650331-Q1

Tool/software:

I would like to get support to have PMIC to supply for  LP5 (PMIC5200), the detail is as below:

Reason to have 2 PMIC solution is due to the board space

PMIC 1

 Buck out 1 = 1.05V

Buck out 2 =0.5V

LDO out = 1.8V

PMIC 2 

 

Buck out 1 =1.8V

Buck out 2 =0.9V

LDO out = 1.0 V