Other Parts Discussed in Thread: LMG5200
Tool/software:
Hello,
I have a question about the different ground potentials of the Evaluation Board. As I see from the schematic, GND and PGND should not be connected anymore if I desolder R10. The Half-Bridge Power Stage (LM5200) can be used for isolated applications.
However, after desoldering R10, I still measure a connection (short) between GND and PGND without anything connected to the Evaluation Board. The board has not been used before. Do I need to disconnect other components from the board so that GND and PGND are no longer connected?
Best regards,
Max