Other Parts Discussed in Thread: TL431
Tool/software:
Is it possible to use the TL431-Q1 shunt regulator as a supercapacitor balancer?
I have a 12V supply with the output current limited to 100mA . If I understand this correctly, I should be able to use the TL431-Q1 to clamp the supercapacitor voltages to 2.5V (less than the 2.7V rating) while they are charging up. Once they are fully charged, they should be balanced to ~2.4V, at which point the TL431-Q1 should only conduct the quiescent current. Effectively this is using the TL431-Q1 as a zener diode replacement for more precise balancing voltage clamping.