Part Number: DRV8837
Other Parts Discussed in Thread: DRV8213EVM, DRV8213
Tool/software:
Hello,
I'm currently using a DRV8837 in my design.
I evaluated a DRV8213EVM for its current regulation capabilities and really liked what the GUI was able to do with the PWM ramp up.
Therefore, I am attempting to duplicate the PWM ramp up in the DRV8213EVM with the DRV8837 chip by monitoring the DRV8213EVM's IN1 and IN2 signals.
First question - the frequency selected on the GUI (50kHz) does not represent the frequency of what is monitored (25-50Hz) on IN1 and IN2 for the DRV8213EVM.
Secondly, even when I have the DRV8837's IN1 and IN2 identical to the DRV8213EVM, and turning off the current monitoring and regulation features of the DRV8213EVM - I am noticing that the DRV8213EVM's start up current is much lower than the DRV8837's (with the same load, VM bulk capacitors, etc). Is there something fundamentally different about the DRV8213 that is not in the DRV8837 that allows it to have a better PWM ramp?