This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2662: +24 and -24 V sensor supply protection (TPS2662)

Part Number: TPS2662
Other Parts Discussed in Thread: TPS2661

Tool/software:

I am connecting more than 20  high voltage current and voltage  sensor to my board all need dual power supply +/-24V. Due to any sensor failure , miswiring, misconnection short other  sensor should get the power and i should get the power supply failure fault signal to that particular sensor .I need device to fulfill the following hardware requirement : 

  1. Sensor Power Supply protection Dual Power Supply +24 V and -24 V.
  2. Need Protection in both polarities of  power supply.
  3. Should get the sensor power  supply fault signal if any  sensor get failed.
  4. Sensors are voltage and current sensor for traction converter.
  5. Should have emi/emc  transient compliance
  6. Shall not have 8-10 pins
  7. Current protection setting shall be settable from external  resistor.
  8. Minimum current limit  setting can be as low as 20 mA.
  9. Protection of both 24V and -24VC is required.
  10. Shall handle the hot swapping , in case sensor connected to that particular power supply connector.
  11. Part which is used in Railway or automatic sensor.

Can i connect  negative to GND of IC ? in this case supply range will be considered as 48 Volt.