Other Parts Discussed in Thread: TPS63806
Tool/software:
Hello,
I have an application where I'm boosting a 3.6V input to 5V output.
Typically the output current consumption is <1mA however I have peaks of 2.5A continuous that last a few seconds.
I noticed that the description of this IC was that the output maximum is nominally "2A".
Looking at Figure 10-2 of the datasheet it appears like I should be OK to draw 2.5A from the IC and still be within recommended operating specifications. Am I understanding this correctly?
If I attempt to draw more than ~2.6A I would expect the IC's current limit to kick in and not damage the IC.
Am I understanding the functionality of this IC correctly? Any other gotchas?
Thanks