Part Number: UCC28060
Tool/software:
Please tell me the contents of the test mode when HVSEN < 0.8V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello user5800825,
This information is not available, however, special test mode are often used during automatic testing of the IC to measure or trim an internal parameter, or program a function.
In normal use of the UCC28060, it is expected that the voltage applied to HVSEN will be > 0.8V.
Regards,
Ulrich
Hello,
Please describe the abnormal behaviors that you are encountered.
Dropping HVSEN below 0.8 V puts the UCC28060 into a special test mode, used only for factory testing. It will not cause harm to the pin, but functionality change to the IC is not disclosed. Please do not attempt to interrogate the IC in this mode as the functionality cannot be guaranteed.
Best,
Hello user5800825,
From information that I found, HVSEN = 0V enables a test mode where the Brown-out time delay (normally 440ms) is reduced considerably, and the 210us restart timer is disabled completely. So if switching stops in a channel, it will not be restarted.
Regards,
Ulrich