This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Driver for Voice Coil Motor

Guru 16770 points

Other Parts Discussed in Thread: DRV201, DRV8881

Hi

We are looking for a VCM driver that meets the following.

VCC:12V-15V

INPUT: Analog Input. 1.8Vpp/2KHz (almost sine wave).

OUTPUT: 3.5Vpp, 1A.

DRV201 is a special driver for VCM but it does'n have analog input.

Do you have an idea to drive VCM in the other way?

Is it possible to drive VCM normal operational amplifier?

regards