This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27220: External NTC reporting different temparature depending on current

Part Number: BQ27220


Hi

I'm currently testing the accuracy of the external NTC temparature reading of the BQ27220 and found that the temparature differs by almost 2 degrees Celcius depending whether the battery provides 10mA or 1800mA.

Setup: 

External temparature 40 C, LiFePO, 95% charged

(1) I_BATT = 1800 mA, V_BATT = 3.1V   --> Temp_NTC  = 28.9 C (already converted from 0.1K)

(2) I_BATT =        9mA, V_BATT = 3.25V  --> Temp_NTC = 37.1 C

 The internal NTC reading also behaves similarly, but not as much as the external one.

Thanks for feedback on this behavior,

Mark