Part Number: ADS7957EVM-PDK
Other Parts Discussed in Thread: ADCPRO, ADS7957
Am I getting real measured values, or something in a "canned" program?
I have the EVM-PDK running with results being displayed in ADCPro. Results are impressively good. So, I tried to verify inputs and outputs (analog and digital). I connected a scope to pins on connectors P1 and P2. But I can not find ANY signals (analog on P1, or digital on P2) while in the acquire mode. I used the EVM-PDK's user's Guide (slau262d.pdf) schematic on p.27 (and some DVM probing to determine orientation).
ADS7957 is 1MSPs 12-bit 16 channel
Details of ADCPro setup:
EVM = Triple generator sampling 44100 SPs; Ch 1=Sine, resolution = 16 (?), V=+15V, -15V (?) Codes= +32767 & -32768 (?), freq=10kHz, Amplitude= 0 dBFS. I assumed CH0 or Ch1 would be stimulated.
Test - Multi FFT, 2048 samples, Block Size=16384.
Please help with how to find the signals. Otherwise, I suspect the converter is not really being exercised in the 'EVM-PDK.
Thanks!