Part Number: TWL6032
Other Parts Discussed in Thread: TPS65950
Hi team,
I received a question about TWL6032 RTC accuracy from my customer
Customer is using TWL6032 for their products, but it seems that there is a large time lag on RTC. Therefore, customer wants to know the accuracy of the RTC.
The datasheet doesn’t describe the RTC accuracy, so could you tell me it?
If possible, could you show the accuracy as following example?
For example : The RTC will shift XX seconds for YY months under the ZZ conditions.
Customer requested me to show it with several conditions.
Regarding temp range, the application would not be used at too high temp/too low temp.
Therefore, it is helpful that the temp range is under use environment(e.g. 0degC ~ 45degC).
Customer mentioned that input clock is 32.768kHz, and the frequency deviation is +-20ppm including temp deviation.
Customer thinks that there is no problem for input clock.
Regards,
Yamaguchi