Hello!
I work with Atmega 1280 microcontroller and TI ads8320 ADC.
The appearance of the installed ADC and oscillograms are attached.
The input measured signal is a stable DC signal, it was checked using 34401A Agilent digital multimeter.
The supply and reference inputs are both provided with 2 ceramic capacitors 10 uF and 0.1 uF.
I can’t obtain good spi communication of the microcontroller with the ADC.
The frequency is 125 kHz. When applying clock pulses and a low signal to CS for 22 cycles,
and another 4 cycles after the signal to CS becomes high,
an unstable and very strange signal is observed at the output of the ADC.
I can not understand why) in accordance with the datasheet everything should work)!!
This is the second way I used.
The images from the oscilloscope are static images. In dynamics, the code coming out of the ADC is very unstable. Measurement results vary in jumps.
This is an image of how I placed the ADC.