Part Number: TX810
Hello,
I have an electroacoustic transducer driver of capacity 60W electrical and 10W acoustical. Its internal impedance is 16 ohm. This driver is enabled to transmit and receive the signal. I need a simple switching device that will Turn ON the power amplifier signal to the transducer for 1 second and Turn ON the preamplifer path for 9 seconds and continue likewise. I have seen TX810 T/R switch, it's an 8 channel programmable switch. Is this switch can work for me? Also, there are other switches as well so which switch can be most suitable for my application?