Part Number: LM43602-Q1
I have a LM43602-Q1 converter that is converting 12V to 5V and running at 500kHz. We are seeing a large amount of EMI that appears to be coming specifically from the boost cap. Waveforms from each side of the cap shown below. If we relocate the cap, the EMI follows the cap. We also tried larger values of capacitance.