Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: SMBus Rise/Fall Time Definition

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQ29312, BQ20Z80, , BQ40Z50

Hello TI Team,

I'm working on a design using BQ40Z50-R2 to replace BQ20Z80+BQ29312 chip set. When I look up the datasheet for SMBus rise and fall time, I found the test condition for rise/fall time are different.

If using VDD = 3.3V,

For BQ20Z80: Rise is 0.8V ~ 2.97V , Fall is 2.25V ~ 0.65V;

For BQ40Z50-R2: Rise is 0.32V ~ 2.97V, Fall is 2.97V ~ 0.32V.

It looks like the voltage range is wider for BQ40Z50-R2. How to understand the voltage range and its changing?  Does wider range mean that BQ40Z50-R2 has maybe quicker response? Also, the old device and its host were designed based on BQ20Z80's range. Will wider voltage range be an issue to the host?

I would appreciate it very much for you help!

Best Regards,

Zhihan

  • Hello Zhihan,

    The wider range shouldn't be an issue for the host, I'm not sure of the reason for the switch but the SMBus driver has been updated since the older the gauges so the communication will be more reliable. The speed is only related to the clock frequency of the communication.

    Sincerely,

    Wyatt Keller

  • Hello Wyatt Keller,

    Thank you so much for your response!

    For the voltage range, I guess my question is which one should we use for the timing verification? Because when measuring the same rise edge, narrower range would definitely have shorter rise time. So what if for example, the rise time is < 1000ns with narrower range while > 1000ns with wider range. Will this be considered as PASS or FAIL? Or should we just keep the same criteria as how the host device is design, for example, host design is based on narrower range?

    Also for the clock frequency, does BQ40Z50-R2 has additional tolerance regarding the max frequency of 100kHz? The host currently has nearly 100kHz, but we suspect the frequency may sometimes exceed 100kHz. So we wonder how tolerant is the IC when frequency exceeds 100kHz? And if possible, do you have any distribution data on the frequency tolerance margin?

    Thank you again!

    Zhihan

  • Hello Zhihan,

    I'm not sure I follow your question, I would just reference the datasheet for the host and the gauge to see if they are both within the required range.

    The BQ40Z50 has 2 modes for the SMBus, there is a faster mode in the range of 40kHz to 400kHz. The communication circuitry is fairly robust in the gauges, but like I mentioned if it will be exceeding 100kHz substantially you should use the other mode.

    Sincerely,

    Wyatt Keller

  • Hello Wyatt Keller,

    Thank you for your response and sorry for the confusion.

    For the voltage range, I mean for the old IC + old host, our timing test was based on the old narrower range. As long as the narrower range time is within SMBus spec, then it's good. But now for the new IC + old host, for the timing test, which range should be our pass/fail criteria?

    For the SMBus, we may try on the faster mode. Thanks for the tip!

    Best Regards,

    Zhihan

  • Hello Zhihan,

    The best way is to use the smbus 2.0 or 3.0 specification and measure the rise and fall times corresponding to what the spec recommends.

    Thanks!

  • Hello Kang Kang,

    Thanks for reply!

    I'm still a little bit confused. Since BQ40Z50-R2 is SMBus v1.1, should we follow the range defined in SMBus 1.1 rather than 2.0 or 3.0? Especially the range is different between 1.1 and 2.0.  And 2.0 is the same as 3.0.

    Another question is regarding SMBus fast mode in BQ40Z50-R2. In addition to set SBS Configuration "XL", do we need any hardware change or hardware requirement on the comm line since the frequency is increased? And also, with larger frequency, will we also need to adjust the rise time/fall time criteria for verification?

    Thanks,

    Zhihan

  • Hello Zhihan,

    Got it. You should follow SMBus v1.1.

    For higher frequency, 400 kHz, you will want to look at the bus capacitance and pull-up resistance.

    Thanks!

  • Hello Kang Kang,

    Thank you for your reply!

    Just one more question regarding 400kHz mode. Does TI have any recommendation on the schematic especially for SMBus lines, such as resistor and ESD diode?

    Thanks,

    Zhihan

  • Hello Zhihan,

    ESD diode depends on your ESD requirements of the system. We have it on our EVM design.

    The pull-up resistor is something you will need to determine based on rise and fall time and IOL, VOH, VOL requirements.

    Thanks!