This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3707: VL and VH

Part Number: UC3707


Hi sir,

I wanna use UC3707 for VIN = VC = 40V condition.

The signal input (input A, input B) will be supplied from the FPGA,

but what are the digital input low level and digital input high level at 40V?

The data sheet has only 20 V conditions.

Digital input low level Max 0.8V
Digital input high level   Min 2.2V

The same to 20 V conditions? or other condition.

Hope you can clarify this query.

Thanks.

Regards,