A recently released report from a consulting professor at Stanford University identifies that the growth in electricity use in data centers over the years 2005 to 2010 is significantly lower than the expected doubling based on the growth rate of data centers from 2000 to 2005. Based on the estimates in an earlier report on electricity usage by data centers, worldwide electricity usage has only increased by about 56% over the time period of 2005 to 2010 instead of the expected doubling. In contrast, the growth in data center electricity use in the United States increased by 36%.
Based on estimates of the installed base of data center servers for 2010, the report points out that the growth in installed volume servers slowed substantially over the 2005 and 2010 period by growing about 20% in the United States and 33% worldwide. The installed base of mid-range servers fell faster than the 2007 projections while the installed base of high-end servers grew rapidly instead of declining per the projections. While Google’s data centers were not able to be included in the estimates (because they assemble their own custom servers), the report estimates that Google’s data centers account for less than 1% of electricity used by data centers worldwide.
The author suggests the lower energy use is due to impacts of the 2008 economic crisis and improvements in data center efficiency. While I agree that improving data center efficiency is an important factor, I wonder if the 2008 economic crisis has a first or second order effect on the electricity use of data centers. Did a dip in the growth rate for data services cause the drop in the rate of new server installs or is the market converging on the optimum ratio of servers to services?
My data service costs are lower than they have ever been before – although I suspect we are flirting with a local minimum in data service costs as it has been harder to renew or maintain discounts for these services this year. I suspect my perceived price inflection point is the result of service capacities finally reflecting service usage. The days of huge excess capacity for data services are fading fast and service providers may no longer need to sell those services below market rate to gain users of that excess capacity. The migration from all-you-can-eat data plans to tiered or throttle accounts may also be an indication that excess capacity of data services is finally being consumed.
If the lower than expected energy use of data centers is caused by the economic crisis, will energy spike up once we are completely out of the crisis? Is the lower than expected energy use due more to the market converging on the optimum ration of servers to services – if so, does the economic crisis materially affect energy use during and after the crisis?
One thing this report was not able to do was ascertain how much work was being performed per unit of energy. I suspect the lower than expected energy use is analogous to the change in manufacturing within the United States where productivity continues to soar despite significant drops in the number of people actually performing manufacturing work. While counting the number of installed servers is relatively straightforward, determining how the efficiency of their workload is changing is a much tougher beast to tackle. What do you think is the first order affect that is slowing the growth rate of energy consumption in data centers?
Visit Embedded Insights to see the full conversation occurring across multiple communities about this and other questions of the week.