Latest member of the Droid family brings even greater experiences to life
Blogs and industry sites have been overflowing with anticipation over the past few months about the launch of the Droid X, Motorola’s second-generation Droid smartphone. Today, we applaud Motorola’s official launch of this eye-catching device! As the Applications Engineering Manager, I worked on the OMAP™ processor team that supported this project. And, I wanted to share some thoughts with you about today’s news.
Building on the success of the first Droid, Droid X promises the next level of performance and power capabilities. You can check out Motorola’s press release for complete specs. As CEO Dr. Sanjay Jha stated in his presentation today, Droid X also features some key TI components that make its features come to life:
-
OMAP3630 processor for enhanced processing capabilities at low power levels: The OMAP3630 processor, based on a solid ARM® Cortex™-A8 foundation, addresses Droid X’s high-performance needs at the low power levels required to support multitasking, data-intensive apps and rich multimedia. The 45-nm OMAP3630 processor runs at a higher frequency than its predecessors, while lowering core voltage and adding power reduction features. The OMAP3630 processor works together with a companion power-management device, also from TI, to establish these low power sips. What does this mean for Droid X? The step up to the OMAP3630 processor fuels:
-
Up to a 2X increase in ARM and graphics processing performance as compared to Droid, at up to 2X lower power levels.
-
Power-optimized, dedicated engines that allow unparalleled multimedia experiences at 1GHz, as compared to 550MHz found on Droid.
-
Features like 720p HD record and playback, including HDMI support to hookup to an HDTV, and an 8-megapixel camera utilizing on-board ISP technology from TI.
-
-
WiLink™ 6.0 solution for robust connectivity: Optimized to work with TI’s OMAP 3 processors, the WiLink 6.0 solution provides the strong connectivity support that brings Droid X experiences to life. By integrating mobile WLAN, Bluetooth® and FM solution on a single chip, the WiLink 6.0 solution solves coexistence problems between technologies to deliver seamless connectivity for the rich apps – like Internet browsing, streaming and downloads – that consumers rely on.
We couldn’t be more thrilled to be inside such another ground-breaking device from Motorola. As you know, Motorola issued the first Droid in October 2009, which featured TI’s OMAP3430 processor and WiLink 6.0 solution as well. TI is excited to be part of the second-generation Droid X, as the Droid family leaves a solid mark on the mobile market and in the Android world.
What makes you excited about this device? Let us know what you think by posting a comment here, or connecting with us on Twitter: @TXInstruments.
Link to Motorola’s press release: http://mediacenter.motorola.com/content/detail.aspx?ReleaseID=12976&NewsAreaId=305