<?xml-stylesheet type="text/xsl" href="https://e2e.ti.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>Overlooking the obvious: the input impedance of a difference amplifier</title><link>/blogs_/archives/b/precisionhub/posts/overlooking-the-obvious-the-input-impedance-of-a-difference-amplifier</link><description>Monolithic difference amplifiers are integrated circuits that incorporate an operational amplifier (op amp) and four or more precision resistors in the same package. They are incredibly useful building blocks for analog designers who need to convert </description><dc:language>en-US</dc:language><generator>Telligent Community 13</generator><item><title>RE: Overlooking the obvious: the input impedance of a difference amplifier</title><link>https://e2e.ti.com/blogs_/archives/b/precisionhub/posts/overlooking-the-obvious-the-input-impedance-of-a-difference-amplifier</link><pubDate>Sat, 04 Sep 2021 03:08:55 GMT</pubDate><guid isPermaLink="false">cb01d8b2-d089-468d-babb-77d1d8683490:e5656368-4543-4249-a31b-ac00ed72e0ed</guid><dc:creator>Steve O&amp;amp;#39;Connor</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;Hi, I like this post, however doesn&amp;#39;t Equation 7 mean that R&lt;sub&gt;in(N)&amp;nbsp;&lt;/sub&gt;could be negative.&lt;/p&gt;&lt;img src="https://e2e.ti.com/aggbug?PostID=667671&amp;AppID=930&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: Overlooking the obvious: the input impedance of a difference amplifier</title><link>https://e2e.ti.com/blogs_/archives/b/precisionhub/posts/overlooking-the-obvious-the-input-impedance-of-a-difference-amplifier</link><pubDate>Thu, 07 Nov 2019 18:06:17 GMT</pubDate><guid isPermaLink="false">cb01d8b2-d089-468d-babb-77d1d8683490:e5656368-4543-4249-a31b-ac00ed72e0ed</guid><dc:creator>tim hughes</dc:creator><slash:comments>1</slash:comments><description>&lt;p&gt;John, &amp;nbsp;the incremental impedance DeltaV/DeltaI when looking into the positive input is R3+R4 the same as you state, but the corresponding incremental impedance is just R1 when looking into the diff amplifier&amp;#39;s negative input because the R1- R2 node is at virtual earth . &amp;nbsp; Direct DC &amp;nbsp;V/I &amp;nbsp;values rather than impedance= DeltaV/DeltaI is what you are discussing above.&lt;/p&gt;
&lt;p&gt; For example, the case you indirectly mention where you want to make an AC coupled differential amp and you need to know the impedance when putting Capacitors in series with the inputs you need to to use the above mentioned incremental impedances and make the time constants R1C1 = (R2+R3)*C2 to achieve reasonable common mode rejection through balanced input time constants. (C1 is in series with R1,C2 in series with R3). &lt;/p&gt;
&lt;p&gt;( In practice because you cant match capacitors much better than about 1%, CMRR at low frequencies wont be better than 40dB if you are lucky. ) &lt;/p&gt;
&lt;p&gt;For a concrete example for the case of &amp;nbsp;all equal resistors R1 to R4 then C1 must be twice as large as C2 and the -3dB cutoff will be 1/2*pi*R1*C1 (or equivalently = 1/2*pi*C2*(R3+R4) . &amp;nbsp;&lt;/p&gt;
&lt;img src="https://e2e.ti.com/aggbug?PostID=667671&amp;AppID=930&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: Overlooking the obvious: the input impedance of a difference amplifier</title><link>https://e2e.ti.com/blogs_/archives/b/precisionhub/posts/overlooking-the-obvious-the-input-impedance-of-a-difference-amplifier</link><pubDate>Tue, 08 Sep 2015 22:20:13 GMT</pubDate><guid isPermaLink="false">cb01d8b2-d089-468d-babb-77d1d8683490:e5656368-4543-4249-a31b-ac00ed72e0ed</guid><dc:creator>John Caldwell</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;Hi Ken,&lt;/p&gt;
&lt;p&gt;Thanks for bringing this to our attention. To me, the INA133 datasheet is correct and the INA134 datasheet may need to be updated. We can calculate the common-mode input impedance pretty quickly using the equations in the above post. First, if we have a common-mode voltage source the input impedance it &amp;quot;sees&amp;quot; looking into the INA134 is RIN(N) in parallel with RIN(P) &amp;nbsp;(You can imagine tying the two inputs together and then applying a voltage source to them). As usual RIN(P) is 25k + 25k = 50k. RIN(N) in this case is a bit different, since VIN(P) = VIN(N), then VIN(P) / VIN(N) = 1, and equation 7 simplifies to RIN(N) = R1 / 0.5 = 50k. Since RIN(P) is in parallel with RIN(N) for common mode voltages, 50k || 50k = 25k. The differential input impedance can be done &amp;quot;by inspection&amp;quot; by remembering that there is a &amp;quot;vitual short&amp;quot; between the two op amp inputs, and therefore R1 and R3 are in series for differential input voltages, 25k + 25k = 50k. &lt;/p&gt;
&lt;img src="https://e2e.ti.com/aggbug?PostID=667671&amp;AppID=930&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: Overlooking the obvious: the input impedance of a difference amplifier</title><link>https://e2e.ti.com/blogs_/archives/b/precisionhub/posts/overlooking-the-obvious-the-input-impedance-of-a-difference-amplifier</link><pubDate>Tue, 08 Sep 2015 20:44:14 GMT</pubDate><guid isPermaLink="false">cb01d8b2-d089-468d-babb-77d1d8683490:e5656368-4543-4249-a31b-ac00ed72e0ed</guid><dc:creator>Ken Dillinger</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;Because I like being &amp;quot;that guy&amp;quot;, there seems to be a problem with the INA134 datasheet. &lt;/p&gt;
&lt;p&gt;The &amp;nbsp;INA133 datasheet which has the same value of resistors for the network (25kohm), but states the the common-mode input resistance as 25kohm and the differential input resistance as 50kohm.&lt;/p&gt;
&lt;p&gt;The only clue is that for the INA133 the common-mode voltage is specified at VCM=0. So, I presume, that means the input resistance is simply the resistor on the inverting node. If driven from a transformer or other floating source the differential impedance of 50kohm makes sense.&lt;/p&gt;
&lt;p&gt;The INA134 has 25kohm resistors for the network and the datasheet specifies 50kohm for both common-mode and differential input &amp;nbsp;resistances. &lt;/p&gt;
&lt;p&gt;I always presume people are smarter than me or I missed a subtle clue, but this looks inconsistent.&lt;/p&gt;
&lt;p&gt;-Ken&lt;/p&gt;
&lt;img src="https://e2e.ti.com/aggbug?PostID=667671&amp;AppID=930&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: Overlooking the obvious: the input impedance of a difference amplifier</title><link>https://e2e.ti.com/blogs_/archives/b/precisionhub/posts/overlooking-the-obvious-the-input-impedance-of-a-difference-amplifier</link><pubDate>Mon, 17 Aug 2015 07:15:30 GMT</pubDate><guid isPermaLink="false">cb01d8b2-d089-468d-babb-77d1d8683490:e5656368-4543-4249-a31b-ac00ed72e0ed</guid><dc:creator>Haroldo Amaral</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;Hi, Excellent post.&lt;/p&gt;
&lt;p&gt;The same analysis can be used with other configurations.&lt;/p&gt;
&lt;img src="https://e2e.ti.com/aggbug?PostID=667671&amp;AppID=930&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>