Offset Voltage and Open-Loop Gain—they’re cousins

Everyone knows what offset voltage is, right? In the simplest G=1 circuit of figure 1a, the output voltage is the offset voltage of the op amp. The offset voltage is modeled as a DC voltage in series with one input terminal. In unity gain the offset is passed directly to the output with G=1. In the high gain circuit on the right the output voltage is 1000∙Vos, right?

Well, nearly so, but not quite. Understanding the “not quite”can help you understand errors in your op amp circuits.

In the first case the output voltage was very near mid-supply (we’re assuming ± supplies). This is the output voltage at which we define and test offset voltage. But in the second case, the output may be several volts, assuming  several millivolts of offset. That requires a small additional differential voltage at the input of the op amp to create that output swing (according to open-loop gain of that amplifier). Let’s do some numbers:

If the DC open-loop gain is 100dB, that amounts to 1/10^(100dB/20) = 10uV/V. So for every volt of output swing from mid-supply, the input voltage must change by 10uV. Think of it as an offset voltage that changes with DC output voltage. With 9 volts of output swing it’s 90uV change. Maybe that’s insignificant in your circuits. Maybe not.

The point is that thinking of finite open-loop gain as a changing offset voltage with a change in output voltage provides an intuitive way to size up the error. And the character of that error may matter, too. To test offset voltage and open-loop gain, we use a fancy two-op loop circuit. With it we can control the output voltage and measure the offset voltage. If we sweep the output voltage through its full output range the change in offset voltage often looks something like figure 2.

Note that the greatest change in offset voltage tends to occur at the output extremes, near the positive and negative rail. The op amp is “straining” to produce its maximum output. The incremental open-loop gain is higher in the middle and falls near the output nears the rails. As you plan your circuits, expect that this is the case. Offset voltage will increase more dramatically as you push the op amp to its swing limits.

Not all op amp manufacturers specify AOL the same way. Our precision op amps are tested for open loop gain, averaged over a generous output swing range for good linear operation (the red line in figure 2). In the spec table it looks like this:

When the amplifier is overdriven (creating a larger offset voltage) the output will swing closer to the rails. Sometimes we show output swing that differs from the conditions in table A.  The output swing in table B, for example, shows the output voltage with the input overdriven. This is affectionately known as a or “slam spec” in our op amp development group, meaning that the input is overdriven and slammed as far as it can go to the rail.

Both types of specs are useful, depending on the requirements of your application. The key is to understand and carefully interpret the specifications.

Thanks for reading and comments welcome.

Bruce           email:  thesignal@list.ti.com

           Index to all The Signal blogs.

Anonymous
Parents
  • Hi Bruce

    Would a more correct model of Input Offset Voltage be (Vos + Vo/AOL) in series with the non-inverting op amp input rather than just Vos as sometimes depicted in text books?  (Vos is the Input Offset Voltage for Vo=0V, Vo is output voltage and AOL is of course open-loop gain)

    regards

    Steve

Comment
  • Hi Bruce

    Would a more correct model of Input Offset Voltage be (Vos + Vo/AOL) in series with the non-inverting op amp input rather than just Vos as sometimes depicted in text books?  (Vos is the Input Offset Voltage for Vo=0V, Vo is output voltage and AOL is of course open-loop gain)

    regards

    Steve

Children
No Data