Audio loudness and quality evaluations for smart amplifier solutions

Other Parts Discussed in Post: TAS2555

Making transducers sound as natural as possible is quite a challenge for audio tuners. While subjective evaluations help designers fine-tune sound, they face several challenges, such as visual cues impacting both audio perception and quality.

Objective measurements help mitigate some of the challenges posed by subjective evaluation. Objective evaluations also help when making A/B comparisons. When conducting objective or subjective tests, audio tuners prefer high-quality audio recordings over highly compressed MP3/AAC files. Raw WAV files are the best.

To perform objective analyses, you need a good-quality microphone; an audio sound card to capture the microphone data to your PC; and software tools like MATLAB, Audacity and Room EQ Wizard (REW).

Figure 1 depicts an experimental setup using the TAS2555 audio amplifier, a TI SmartAmp.

Figure 1: Typical lab setup for audio measurements

These are some of the objective parameters that can help audio tuners judge the perception of audio loudness and quality.

Loudness
One of the main objectives of TI’s TAS2555 is to drive the speaker to its maximum limits while protecting it against electrical or mechanical failures. The peak and average sound pressure level (SPL) measurements help determine this objectively.

I use REW for an analysis like the one shown in Figure 2, which also uses the TAS2555 audio amplifier to analyze a popular rock song.

Figure 2: SPL measurements

Timbre
It is imperative that while your solution should sound as loud as possible, it should not be at the expense of audio quality/timbre.

Audio timbre/quality represents the characteristics of music reproduction, which allows the human ear to distinguish sounds that have the same pitch and loudness. Timbre is directly related to static parameters like harmonic content and dynamic parameters like vibrato and the attack-decay envelope. The Acoustical Society of America (ASA) definition of timbre describes it as an “attribute of auditory sensation which enables a listener to judge that two nonidentical sounds, similarly presented and having the same loudness and pitch, are dissimilar,” adding that “… timbre depends primarily upon the frequency spectrum, although it also depends upon the sound pressure and the temporal characteristics of the sound.”

Although timbre is highly subjective parameter, audio researchers have tried relating subjective experiences to physical phenomena (objective parameters). Table 1 illustrates this mapping.

Table 1: Mapping subjective experiences to objective parameters

The subjective analysis is objectively possible by studying the tracks (the input being the raw file/audio captured from the reference system vs. the output being speaker audio captured via mic) with these parameters:

  • Global energy. You can compute the global energy of signal x simply by taking the root average of the square of the amplitude, also called root-mean-square (RMS) (Equation 1). In case of an A/B comparison, where the aim is to match the two solutions, the difference between the global energy of the two solutions should be as close as possible to zero.

 (1)

  • Key strength. Key strength in a given musical score is extractable through cross-correlation against the distribution of energy along the various pitches. If the speaker maintains the tonality of the music well, then the key strength estimated in the input file should match that of the file recorded using the mic that captured the speaker output.
  • Audio brightness. The brightness parameter indicates the evolution of brightness throughout a piece of music. High values indicate moments in the music where most of the sound energy is on the high-frequency content, whereas low values indicate moments where most of the sound energy is on the low-frequency content.
  • Energy roll-off. One way to estimate the amount of high frequency in a signal is finding the corner frequency below which a certain fraction of the total energy is contained. The lower the value returned, the darker the content, or the smart amplifier has been able to preserve the low and mid frequencies well.
  • Audio roughness. The roughness indicates the amount of sensory dissonance at each successive moment throughout a piece of music. The sensory dissonance corresponds to a “beating” phenomenon, where several sounds are heard with nearly the same frequency but with just a few hertz difference. Higher roughness makes the sound feel harsher.
  • Audio flatness. Spectral flatness, also known as Wiener entropy, is a measure used to characterize an audio spectrum. Spectral flatness provides a way to quantify how noise-like a sound is, as opposed to being tone-like. The meaning of tonal in this context is in the sense of the amount of peaks or resonant structure in a power spectrum, as opposed to the flat spectrum of a white noise. You can calculate spectral flatness by dividing the geometric mean of the power spectrum by the arithmetic mean of the power spectrum (Equation 2).
(2)

I used the TAS2555 as my example because it can use PurePath™ Console software, which helps you tune the solution to meet your signature sound. PurePath™ Console software is an easy-to-use audio-development suite that helps you evaluate, configure and debug audio products during development. Access to PurePath™ Console software enables you to identify issues and ensure the best possible sound.

TAS2555 vs. coventional solution
Table 2 shows the average values of timbre parameters for measurement across 18 different tracks from various music genres (blues, rock, classical).

Table 2 - Comparison of objective parameters between TAS2555 and a popular phone

Tuning an audio solution to get the most natural sound possible is often hard and takes a lot of time. There are several tools out there to help with this process; however, it is important to make sure that you account for (and correct if needed) the elements of sound that I’ve covered in this post. If you have had similar problems in the past, please leave a comment below. How do you fine-tune your sound?

Additional resources

Anonymous