How can I achieve accurate gain error and drift with a switched-gain transimpedance amplifier?

Other Parts Discussed in Post: OPA3S328

The transimpedance amplifier (TIA) is one of the most common circuits in the world of precision analog circuits. The dynamic range required of a single TIA can be quite a challenge, often spanning many decades, such as picoamperes to microamperes.

 Selecting a single resistor to accommodate such a wide dynamic range is a lose-lose situation, so circuit designers will often turn to an array of switches to select a few different resistor values, depending on the current level measured at the time. The switch on-resistance (RON), drift and nonlinearity do play a significant role in TIA accuracy, however, particularly at lower feedback resistor values.


 Maximize accuracy in your transimpedance amplifier design

amplifier icon Read our application report to learn how to build a low-noise, high-accuracy programmable gain TIA using the OPA3S328.

TI’s OPA3S328 is a dual operational amplifier with integrated switches for transimpedance applications. It includes two wide-bandwidth (40 MHz) low-input bias current precision amplifiers with a multiplexer to select the different gains, and a second set of switches for Kelvin sensing. In this article, I’ll illustrate the advantages of Kelvin sense switching connections over traditional switched-gain TIA circuits.

 This is the second installment in a four-part series discussing how to increase system accuracy and efficiency with operational amplifiers built on TI’s new, proprietary complementary metal-oxide semiconductor precision process technology.

The programmable-gain TIA

It is possible to implement a TIA by cascading a single-gain TIA with a second programmable gain amplifier (PGA) stage. However, a better approach is to incorporate the programmable gain and TIA into a single stage. This approach provides a significant advantage from a noise performance perspective, since the sensor signal is gained on the first transimpedance stage, resulting in lower total output noise.

Figure 1 shows a programmable-gain TIA using the OPA3S328. The integrated 1-to-2 analog switch selects the different transimpedance feedback resistors.

Figure 1: Switched-gain TIA

The feedback resistor (RF) determines the gain of the transimpedance operational amplifier and converts the photodiode current (ID) to a voltage (VOUT) using Ohm’s law, VOUT = IDRF. For an accurate transimpedance current-to-voltage conversion, the amplifier’s input bias current and input offset voltage must be small. The OPA3S328 offers a low offset voltage of ±10 µV and a low-input bias current of ±0.2 pA. The gain resistors are typically decades apart to provide optimal resolution for different ranges of current.

Switch characteristics

Consider the electrical characteristics of the switches when designing the switched-gain TIA. The capacitances and resistances of the switch will affect the bandwidth and stability of the circuit. Furthermore, the RON of the switch can be a source of gain error.

The OPA3S328 incorporates two sets of low-leakage, low-capacitance switches useful for different circuit configurations, including programmable-gain transimpedance applications. The quad flat no-lead package version of the OPA3S328 features switch A in a 1-to-2 matrix configuration and switch B in a 1-to-3 matrix configuration.

Table 1 shows the critical data-sheet switch parameters. 

Parameter

Test condition

Minimum

Typical

Maximum

Unit

CIN

Switch open, INSA/B = 2.5 V

 

3

 

pF

COUT

Switch open, OUTSA/B/1/2/3 = 2.5 V

 

0.7

 

pF

CINOUT

Switch closed, INSA/B = OUTSA/B/1/2/3 = 2.5 V

 

6

 

pF

RON

Switch closed, V+ = 5 V, INSA/B = 2.5 V

 

84

125

Table 1: OPA3S328 switch characteristics

CIN and COUT represent the open switch parasitic switch capacitance, while CINOUT represents the total switch capacitance while the switch is closed. RON is the switch series resistance when the switch is closed. Figure 2 shows a simplified switch model.

 Figure 2: Simplified switch model for the OPA3S328

On the programmable TIA, the voltage error across RON can be significant at the higher photodiode currents.

Figure 3 shows the calculation of the TIA output accounting for the RON voltage drop. In this example, the circuit is powered with a +5-V supply and uses a feedback resistor where RF2 = 2 kΩ, for a maximum photodiode current of 2 mA and a target TIA output of +4 V. The voltage drop across RON is 250 mV, however, and the TIA output has a significant error.

Figure 3: Switch RON and TIA output error

The RON will produce DC gain errors and distortion on the TIA. These gain errors are substantial at lower feedback resistor values. Furthermore, the RON changes with temperature and the switch voltage, producing gain error drift, nonlinearity and distortion. Figure 4 shows the change of RON vs. the voltage difference across the switch.

Figure 4: Switch RON vs. switch voltage

Switch Kelvin sense connections

One way to virtually eliminate or significantly reduce the gain and non-linearity errors due to the switch series resistance is to build a multiplexer using the second integrated switch of the OPA3S328. The multiplexer input senses the TIA output connection for the selected gain right at the RF feedback resistor terminal. The second amplifier stage is configured in a high-impedance noninverting configuration, buffering the multiplexer and providing an accurate Kelvin sense connection of the TIA output for each gain. Since the input bias current of the operational amplifier is minimal, less than 10 pA, the voltage drop across the switch OUTSB2 RON is negligible.

Figure 5 shows the OPA3S328 circuit using switch B in a 3-to-1 matrix configuration to build the Kelvin sense connection multiplexer, buffered with a second-stage amplifier.

 

Figure 5: Switch Kelvin-sense connections and high impedance buffer

The Kelvin sense connections eliminate the gain error, drift and nonlinearity because of the switch RON through the high impedance second-stage amplifier. It is also possible to configure the second stage in a noninverting gain configuration, adding flexibility for higher gains while maintaining circuit bandwidth.

Conclusion

The OPA3S328 dual operational amplifier offers low-input bias current, high DC precision performance, low noise and high bandwidth, making it a good fit for TIA applications. The device incorporates two sets of low-leakage and low-capacitance analog switches useful for the configuration of PGAs in an integrated solution. The OPA3S328 programmable TIA, using analog switches and a Kelvin sense circuit topology, can help eliminate gain error, gain error drift and nonlinearity given the switch RON.

The next installment of this series will discuss how to achieve microvoltage-level precision in thermocouple and thermopile applications.

Additional resources

Anonymous
Parents
  • Thank you, Luis, for this great white paper. Trans impedance amplifiers and current sensing circuits are often used as a TI product show case.
    I think a paper on how this OpAmp could be used to measure a wide range resistance (programmable current source + programmable gain amplifier) or laboratory-grade volt meter (min 10MΩ input) would also be very valuable and interesting.

  • Hi Tomasz,

    Thank you for your comment and interest on the OPA3S328.  Indeed, this is a good application for the OPA3S328.

    We had a internal team discussion sometime ago regarding a circuit to perform a resistance measurement using the OPA3S328.  The preliminary block diagram below shows the OPA3S328 on a programmable current source / programmable gain amplifier circuit for a resistance measurement application.  I will discuss with the team the possibility of developing an application note or reference design.

    Thank you and Kind Regards,

    Luis

     

  •  

    Thank you for sharing this example and comments. An application note on measuring high-range resistance would be highly appreciated.

    Recently I tried to develop solution was aimed at measuring high impedance (10M) voltage (no success yet).
    I have tried to use OPA392 for its super-low bias current and low offset voltage. The obtained 8.31mV error was not impressive. Also, OPA392 in such configuration seems to be difficult to stabilize. R8 and C4 elements have to be carefully selected and they increase stability. Maybe my approach is too simplistic.
    Are you aware of any examples on how to approach such engineering design challenge?

    The link below contains TINA screenshot. For any reason I could not place this image here.
    https://drive.google.com/file/d/1tJ1u_pZGefeXlq1dBETFhpdct-mFG0R_/view?usp=sharing

  • HI Tomasz,

    Thank you for your suggestion for an application note measuring high resistances, I agree this application note would be a useful and will discuss with the team for future development/publication.

    I am unable to see your circuit on this page, since this is a landing page for the OPA3S328 Switchable Gain Transimpedance blog.  If you require technical support with the OPA392 on an impedance measurement circuit, kindly submit a query on the E2E Amplifier's forum page.  You should be able to append the Custom schematic (or simulation files) for review when submitting a new E2E question.  The applications team will be able to assist. 

    Thank you,

    Kind Regards,

    Luis

Comment Children
No Data