System trade-offs for high- and low-side current measurements

Other Parts Discussed in Post: INA180

Measuring current may sound like a simple task, but it is not as easy as it sounds. Current can’t be sensed directly; however, it is related to other measureable parameters that you can sense directly, such as voltage and magnetic field density.

In general, there are two ways to measure current. The first is by measuring the magnetic field density generated around a current-carrying conductor. This method is suitable when you require noninvasive current measurements, but you’ll need to justify its relative high cost and complex implementation. The second is to use a small shunt resistance and measure the differential voltage across it that results from the current flow, a direct implementation of Ohm’s law. This method is common due to its high accuracy and low implementation costs. Figure 1 shows the two different methods and underlying physics behind each.

Figure 1: Current-sensing methods and their underlying physics

In this blog post, I will discuss the resistive-based method that utilizes Ohm’s law across different implementations and present some of their system benefits and tradeoffs.

Depending on the application and use of the current to be measured (protection, system monitoring or control), you can place the shunt resistor either between the supply and the load or between the load and ground. The first placement is called high-side sensing (sensing the current entering the load), while the second placement is called low-side sensing (sensing the current leaving the load). Table 1 summarizes those two approaches.

 

High-side sensing

Low-side sensing

Implementation

Differential input

Single or differential input

Ground disturbance

No

Yes

Common voltage

Close to supply

Close to ground

Common-mode rejection ratio (CMRR) requirements

Higher

Lower

Can detect load shorts?

Yes

No

Table 1: High- vs. low-side sensing

Many engineers choose low-side sensing for cost-sensitive applications. Figure 2a shows the most common approach, using a single-ended operational amplifier (op amp). This approach is easy and inexpensive to implement; however, the main trade-off here is accuracy. With this method, parasitic resistances and the temperature coefficients of the resistive gain network will significantly affect accuracy. You can read more about these errors by looking at the 50mA-20A Single-Supply, Low-Side or High-Side Current Sensing Solution precision reference design and TI TechNote, “External Current Sense Amplifiers vs. Integrated On-Board Amplifiers for Current Sensing.”

Figure 2: Main low-side op amp implementations for current measurements

Another pitfall is that you can’t detect load short faults. You can mitigate the accuracy issues related to ground disturbance and parasitics by using the differential configuration shown in Figure 2b. Accuracy will still be limited by the CMRR and drift of the solution, which are a function of the op amp and the matching of the gain resistors. The better the CMRR and drift, the higher the cost of the solution.

To overcome these issues, TI introduced dedicated current-sensing solutions. The INA180 family of devices is a great example that offers high accuracy for cost-sensitive applications. The INA180 family features a high 350kHz closed-loop bandwidth and a fast 2V/µs slew rate that enable their use in applications such as constant current regulators, power supplies, and motor drives, which benefit from such features. Figure 3 shows the basic application diagram of the INA180 with some key specifications.

Figure 3: INA180 basic application diagram and key features

A current-sensing location varies depending on the application and intended use of the measured current. Low-side sensing is preferable for cost-sensitive applications that can tolerate ground disturbances and load shorts. High-side sensing is preferable when ground disturbances cannot be tolerated and load-short detection is required. Traditional discrete implementations compared to dedicated current sensors tend to have limited accuracy, a bigger solution footprint and a relatively higher cost for the same accuracy level.High-side sensing addresses the issues of load short detection and the need to eliminate ground disturbance. The main challenge is the high common-mode voltage that the amplifier needs to tolerate. This challenge, in addition to the accuracy challenges of discrete implementations and cost trade-offs, pushes design engineers to consider other solutions. Again, dedicated current sensors are the perfect solution because they offer high accuracy, low cost and a high common-mode voltage. The INA180 is another great solution for high-side sensing, as the common-mode voltage of the device can go up to 26V.

The INA180 offers a great combination of performance, solution size and design flexibility at the right price point for cost-sensitive applications that are well suited for the main drivers for new electronic devices – cost, performance and size. To get posts like this delivered to your inbox, sign in and subscribe to Analog Wire.

Additional resources

 

Anonymous
  • Chee,

    The current that you measure is limited by the input bias current, offset voltage, and the noise of the amplifier. The sense voltage generated across the shunt resistor should be higher than the offset voltage seen the input terminal of the amplifier. Also, the sense current should not go below the bias currents of the amplifier. Dedicated current sense amplifiers are good in measuring currents in the mA range.  Having a bigger shunt resistance and a low bias and low noise amplifier will allow lower current measurements. TIA and Instrumentation Amps can measure currents in the uA/nA ranges. Measuring current in the pA range requires charge integration techniques.

  • Hi Motaz, nice article! Just curious, is there a limitation on the range of current that can be sensed using this type of single-ended or differential configuration? For instance, if I want to sense current in the pA range, would the tolerance of the sense resistor be not tight enough anymore to make an accurate current measurement? I guess any input bias current into the op amp and inaccuracy of the sense resistor will both contribute to make pA current measurement no longer possible?

  • Ahmet, ground disturbance effect the accuracy of the output voltage reading as it is referred to the load ground that is not connected through the shunt resistance. Ground disturbance is the continuous shift in the load's ground node potential due to the passing current through the shunt resistance. The higher the current passing through the resistance the higher the shift in the ground potential. Some applications can tolerate this disturbance, but if the system requires high level of accuracy ground disturbances need to be eliminated.  This where high side current sensing is the preferred method to use.

  • Hello, Motaz thanks. Why do we need  eleminating  ground disturbances? What is ground disturbance?