Industry pundits have recently speculated that demand for 100G/400G switches may take off in 2019, prompting optical transceiver module vendors to sample data center switches with high data transmission rates earlier than expected. As data center operators accelerate upgrades in preparation for 5G, demand for 100G/400G transceiver modules will become increasingly robust in the next couple of years. And as transmission data rates in optical modules approach 100 and 400 Gbps, designers must consider the need to monitor and control the components within these modules – such as the photodiodes that receive and transmit optical information.
In this post, I’ll discuss various current-sensing functions in high-bandwidth data communication applications for pluggable optical modules. These pluggable modules remain relatively the same size over time but are expected to pack higher and higher data rates, consume lower power per data rate, operate at lower temperatures, and contain integrated circuits with smaller packages than their predecessors, all while ensuring reliable high-bandwidth communication.
Figure 1 is a block diagram of a typical optical module. Let’s discuss the sections contained within the blue and red boxes within the context of current sensing.
Figure 1: Block diagram of a typical optical module
Receive path feedback control
The blue boxes in Figure 1 highlight the receive path. A precision current-sense measurement within the optical module is necessary for the photodiode control feedback to the microcontroller (MCU) to set the appropriate current based on the link brightness, which in turn sets the gain for the transimpedance amplifier and clock data recovery circuit. In optical modules, PIN diodes or avalanche photodiodes (APDs) are typically used for the receiver optical subassembly. PIN diodes have a wide, undoped intrinsic region between a P-type and an N-type semiconductor region. This wide intrinsic region, which in contrast to an ordinary P-N diode is nonexistent, enables the PIN diode to be perfectly suited for photodetector electronics.
APDs have a very sensitive linear range, forcing module makers to precisely monitor its bias voltage. Another very good reason to monitor the current in an APD is because it will break down quickly at an out-of-range optical power or temperature. Ultimately, a precise current measurement in an APD or PIN diode enables optimal performance and assists in system protection.
Transmit path feedback for laser modulator and laser back monitor diode
The bottom red boxes in Figure 1 highlight the transmit path, specifically for biasing the laser diode. Like photodiodes, laser modulators need to be biased to a specific voltage level for maximum linearity to properly modulate the laser light being generated. An externally modulated laser (EML) must be biased with a negative voltage ranging from 0 V to -3.3 V, which makes it tricky for a current-sense amplifier to monitor because it must generate a positive analog voltage that feeds into the analog-to-digital converter (ADC). Figure 2 shows a representation of this circuit. An accurate current measurement of the laser modulator provides feedback to the MCU through an ADC to set the appropriate current based on the module’s temperature.
Figure 2: Measuring current on a negative voltage bias for EML
Finally, you will need a precision current measurement at the output of the internal back monitor photodiode (highlighted in the farthest-right red box in Figure 1). Since this back monitor photodiode current is directly proportional to the transmit power of the laser diode itself, it is critical to get a precise current measurement.
To summarize, current-sensing amplifiers are required in various locations within the receive and transmit paths of the optical module. A PIN diode or an APD ranges in current between 10 µA and 10 mA, while the bias for an EML may be in the order of 100 µA and 30 mA. The current through the back monitor photodiode is in a similar range as the APD. Current measurements in these ranges can be very challenging, thus requiring a high-accuracy solution.
The new INA190 and INA191 current-sense amplifiers from Texas Instruments incorporate an extremely low input voltage offset (<±20 µV max) and have a sub-nanoampere (0.5 nA typical) input bias – both necessary for high-accuracy measurements at low current levels. These devices also have the capability to be powered down with an enable pin, operate at a low power current (a quiescent current of 70 µA max) and are available in small packages – the INA191 in a tiny chip-scale package (0.8 mm by 1.2 mm). High accuracy, low-power operation and small packaging make the new INA190 and INA191 a good fit for high-performance 100G and 400G optical modules.
Additional resources
- Learn more about the INA190 and INA191 and other solutions.
- Download the INA190 data sheet.
- Order the INA190 evaluation module.
- Check out the reference design for optical modules.
- Read this application note: