Controller Area Network (CAN) systems have traditionally been based around 5-V supplies. However, 3.3-V CAN controllers and transceivers are becoming increasingly popular as well. In this post, I’ll list the top five reasons to use a 3.3V-based setup in your factory automation design and address a couple of questions that typically arise.
Figure 1 shows a typical CAN system involving a CAN microcontroller (MCU), a transceiver and two power supplies. A 5-V supply drives the CAN bus, whereas a 3.3-V supply is used for the CAN controller and I/O pins such as TXD and RXD. While this approach helps minimize power consumption on the controller and for the I/O logic, as you will see shortly, there is room for further improvement.
3.3-V CAN transceivers simplify system design by eliminating the need for a separate 5-V rail. As Figure 2 shows, the setup can run on 3.3V alone. Using only a 3.3-V supply eliminates any potential concerns about two rails ramping up at different rates, any sequencing challenges or having to worry about different signal levels. There is just one rail to keep track of, and all signals are on this one rail.
A simpler system directly translates to multiple benefits. Since you no longer need the 5-V rail, you save the cost of an extra regulator and its associated capacitors. It is also an easy way to save crucial board space. Further, if you use a part from the TCAN33X family, such as the TCAN334, you can use the more compact SOT23 2.8mm X 2.9mm package, instead of the conventional 8-pin SOIC 6mm X 4.9mm package. This alone represents a significant area reduction: more than 70%.
Power consumption also comes down across the board with a single, lower-voltage 3.3-V rail, as shown in Figure 3. In addition to the power savings gained by eliminating the extra regulator, there are significant savings in the transceiver itself, both in the form of lower current and lower voltage.
As you can see, the power savings are nontrivial, with the 3.3-V parts pulling significantly less current in both Dominant and Recessive states, and across load conditions. The lower power dissipation numbers also translate to more relaxed thermal constraints on the system.
A question that immediately comes up with 3.3-V parts is whether the driver section of the transceiver is strong enough to drive the appropriate signal levels on the CAN pins. The short answer is yes! The driver is indeed capable of doing so. The CAN standard requires that the Vod value (the voltage difference between CANH and CANL) in Dominant state be between 1.5V and 3V on a standard load. Intuitively, this is relatively easier to meet with a 5-V supply rail, which offers more headroom. However, by using better process technologies with more efficient transistors (lower RDS(on)), and with appropriate sizing and other good design techniques, the internal voltage drops in the driver are minimal, and you can still meet the Vod specification reliably over process, voltage and temperature corners.
Further, the CAN standard allows for additional voltage margin for transmission losses between a driver and a receiver. For example, in the worst-case scenario, even if a driver transmits a Dominant bit with a 1.5-V swing (the minimum allowed value), the receiver only needs 0.9V (the maximum threshold value) to be successfully acknowledged as a Dominant bit. Thus, in normal mode, the worst-case delta is 0.6V, which still offers good noise margin. In low-power standby mode, where line losses are lower (smaller currents), the receiver maximum threshold is 1.15V, so a driver capable of driving a 1.5-V signal on the bus would still be able to send a Dominant bit successfully, with a 0.35-V worst-case margin.
Although I have discussed only Vod, the same holds true for other parameters as well: 3.3-V transceivers still have to meet all relevant CAN standard parameters to be classified as a valid CAN device.
Another important thing to evaluate is compatibility with existing 5-V networks. Figure 4 shows the typical common-mode bias set point for different transceiver families. There is a <1V common-mode shift between 3.3-V transceivers and their 5-V counterparts. However, as Figure 4 shows, this small shift is well within the common-mode range specified by the CAN standard and therefore does not affect functionality or interoperability.
Communications and Systems (C&S) Group GmbH, a widely recognized third-party organization that certifies transceivers from different companies worldwide for CAN compliance, carried out detailed conformance testing of the SN65HVD234 family. Exhaustive testing of a network of 3.3-V transceivers mixed in with 5-V devices revealed no issues with compatibility or interoperability, and the devices were rated by C& S to be fully compliant.
3.3-V transceivers offer a wide range of benefits: simpler setup, reduced cost, lower power and smaller area compared to their 5-V counterparts. They are fully compliant with CAN standards and also compatible with existing 5-V networks.
To learn more about how to implement 3.3-V CAN transceivers, download the application note, “Overview of 3.3V CAN (Controller Area Network) Transceivers.”
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated