Think of a passenger car as a collection of electronic control units (ECUs) that are distributed across the length and breadth of the car and talk to each other using different networks. When adding more advanced automotive electronics for vehicle-to-everything (V2X), automated driving and vehicle electrification, the number of ECUs increases and the amount of data exchanged grows.
Moreover, the increased number of ECUs has diversified network types, from Local Interconnect Network (LIN) and Controller Area Network (CAN) to higher-speed networks such as Flat Panel Display-Link (FPD-Link), PCI Express (PCIe) and Ethernet.
In a domain architecture, ECUs are categorized into domains based on their function, but the zone architecture is a new approach that classifies ECUs by their physical location inside the vehicle, leveraging a central gateway to manage communication. This physical proximity reduces cabling between ECUs to save space and reduce vehicle weight, while also improving processor speeds.
The domain architecture explained simply
To understand the domain architecture, it helps to start by understanding the five domains in which ECUs are typically categorized based on function, as shown in Table 1.
Skip the introduction on domain architecture, and go straight to zone architecture.
Domain |
ECU function |
Powertrain domain |
Manages the function of driving of a car, including electric motor control and battery management, engine control, transmission and steering control |
Advanced driver assistance system domain |
Processes sensor information and takes decisions to assist the driver, including the camera module, radar module, ultrasonic module and sensor fusion |
Infotainment domain |
Manages entertainment within the vehicle and exchanges information between the vehicle and the outside world, including the head unit, digital cockpit and telematics control module |
Body electronic and lighting domain |
Manages comfort, convenience and lighting functions in the car, including the body control module, door module and headlight control module |
Passive safety domain |
Controls safety-related functions such as the airbag control module, braking control module and chassis control module |
Table 1: ECUs are typically classified into five domains
The ECUs communicate and exchange data over networks that are specific and relevant inside their own domain while also communicating with ECUs in outside domains. Since the network in one domain could differ from the network in another domain, a gateway serves as a bridge.
Figure 1 illustrates a vehicle with a domain-based network architecture. In this figure, there is a central gateway module connected to the different domains in the car. Each domain performs several functions. The domain controller (such as the powertrain, for example) includes gateway function. This domain gateway helps communicate data across the ECUs supporting the relevant domain and from the domain to rest of the vehicle.
The domain controller also incorporates ECUs, which helps minimize system cost by integrating the functionality typically implemented through multiple ECUs. TI’s Jacinto™ 7 processors integrate Arm® Cortex® A-72 cores for raw processing power to handle the data, an Arm Cortex R-5Fs for real-time control and gigabit time-sensitive network (TSN) and Ethernet switch for high-speed networking.
Figure 1: Domain architecture
Introducing the zone architecture
If the car was a room and the ECUs were people gathered in that room to discuss different topics, a domain architecture is equivalent to chaotically arranging those people, causing them to shout to others in their discussion groups across the room.
A zone architecture organizes the ECUs based on their location inside the car and adds a vehicle compute module. The vehicle compute module is a computer with a large processing capacity to perform all computations regardless of function. This architecture could also include a gateway module to manage network traffic.
Figure 2 depicts the zone modules and associated zone satellite modules in different regions of the car, along with the central gateway and vehicle compute modules. TI’s Jacinto DRA82x processors for automotive are tailor-made for gateway systems and include features to move data in the vehicle safely and securely. The DRA82x processor family includes devices with an integrated PCIe switch and Gigabit TSN Ethernet switch, which can be used in compute platforms, central gateways and zone modules.
It is possible to use a low-bandwidth network such as CAN for communication between the different zone modules and the central gateway/compute modules. However, high-speed networks such as Ethernet or PCIe are also a good choice because they provide high reliability and smooth operation in a range of automotive temperatures.
Figure 2: Zone architecture
Power advantages of a zone architecture
Engineers are also taking advantage of this reorganization of ECUs to optimize power architectures – specifically the redesign of smart junction boxes, also called power distribution modules, which distribute power to different loads and ECUs in the vehicle. The power distribution boxes are somewhat specific to the car model, and each power distribution box distributes power to a specific set of loads.
Since most power distribution box designs use relays and fuses, they must be easily accessible if a fuse needs to be replaced. In a zone architecture, the power distribution boxes are distributed so that each zone has its own power distribution unit to power the modules in the corresponding zone.
Figure 3 shows the concept of power distribution in a zone architecture, where you can see the integration of each zone’s power distribution module function with the zone module that manages the network traffic and local zone satellites.
Figure 3: Power distribution modules in a zone architecture
Another advantage is that power distribution module designs can be similar throughout the vehicle. Using semiconductor solutions such as smart high-side switches instead of mechanical relays and fuses enables a more sensible power distribution module design, locating modules closer to the loads instead of farther away so that they are more accessible for replacement.
Tailor-made gateway processors lay the groundwork for zone architectures
![]() |
![]() Read the article |
Conclusion
With the increase in the number of ECUs, the vehicle network has evolved into a domain architecture where the ECUs are grouped based on a related function that each ECU is performing. This has increased network complexity, however. Automotive vehicle designers are now considering the use of a zone-based architecture, which offers the advantage of having a vehicle compute module to control vehicle functions.
Taking advantage of this new network architecture enables you to optimize the vehicle power architecture, specifically considering installation of the local power distribution module in each zone along with the zone module that manages network traffic and zone satellite modules. The new zone architecture will ultimately lead to a harness cable weight reduction, which results in higher fuel efficiency for internal combustion engine-based vehicles and higher driving ranges for battery-powered electric vehicles.