For those of you who don’t know me, let me get the formalities out of the way. I absolutely love digital control! You know, stuff like z-transforms, Kalman filters, nonlinear control, adaptive control and ultimately the ability to customize a power-supply solution.
Before you say anything, let me point out that I know I’m an uber geek – but you have to admit that this stuff can be really cool (and of course, really useful). One of the principle ways that digital control is useful is that you can take a pre-packaged controller and add to it or modify it to meet end-solution requirements that may not have been explicitly envisioned by the original device architects. To that end, digital controllers are a power-supply designer’s dream come true.
But let’s be honest: digital control also has some overhead that some of us don’t like or are just not equipped to deal with. In my opinion, that is where a general-purpose pulse width modulation (PWM) can step in and really shine. These devices have been around for some time, and have in many respects served as the workhorse of the power-supply industry. They have a significant track record of outstanding performance and a long list of proven capability of adapting to a designer’s needs. From this vantage point, PWMs kind of look like the analog controller’s version of digital control. In many applications, this can be exactly what a power-supply designer needs: flexibility without complexity.
For example, take the UC3846 or the UC3525A. Many of you probably cut your teeth in power-supply design using one of these devices. Their continued popularity speaks volumes to their reliability and robustness. From an application standpoint, these devices are routinely used for boost, buck, flyback, forward, full bridge, half bridge, peak current-mode, voltage-mode and input-voltage feed-forward use cases in end equipment such as welding, telecom, industrial, lighting and aerospace. I’m sure many of you are thinking of several other topology/application variations you’ve been able to use these parts for. Their flexibility makes the UC3846 or the UC3525A fundamental power-supply building blocks with which you can create dozens of application variations.
Take a look at what’s under the hood of one of these devices.
Figure 1: UC3846 Block Diagram
You have drivers, control and protection: all of the key must-have elements. Because you have access to the key comparator and amplifier inputs and outputs, you have a tremendous amount of freedom to make the device do precisely what you need it to do. Here are a few examples I can think of off the top of my head:
While that doesn’t necessarily have the same level of flexibility found in digital control, it brings a boat-load of similar flexibility benefits that excite a geek like me.
What kind of uses do you have for general-purpose PWM controllers? What flexibility do you value most in these kinds of devices? I’d love to hear your thoughts on this subject in the comments section.
TI has a large selection of general-purpose PWM controllers to satisfy your every need, from the eight-pin UCC28083 to the automotive-qualified LM25037-Q1.
Additional resources
Good morning Brent, Excellent! I fully agree with you! I love to use the UC3846, UC2525 and UCC28C40 because they are such wonderful ics. Anyone who has not used them, are missing something in life. I hate these complex ics with all functions built in - it leaves me with no joy to do my own mathematics and to allow me my flexibility. That is why I stick to these ics. I recently completed a mains driven Li-Ion battery charger using the UC3846 again - what joy it supplies. Thank you very much. Kind regards, Stephen.
That's terrific Stephan. Keep up the good work!