How to control turn on/off thresholds in voltage regulators using a logic level UVLO

When using a voltage regulator, it often happens that the converter will attempt to regulate the output even before the voltage on its input has reached the acceptable design level.  As a result, in this condition, the converter will demand more current from the power supply, potentially current-limiting the power source. Also, the output voltage during this moment of operation may be out of spec, since the duty cycle of the regulator may be at its maximum value. To avoid this, we can use an under-voltage lockout circuit (UVLO) to set a specific input voltage threshold at which the converter turns on and off. 

 

For most converters, there is either a precision enable or a logic level enable pin on the chip itself.

 

For converters with precision enable, the chip compares the voltage at the enable pin to some set, precise internal voltage reference.  Providing an enable voltage above the internal voltage reference turns the converter on, and applying a lower voltage turns the converter off.  As shown in Figure 1, you can usually use just a voltage divider from VIN to the enable pin to set a precise enable threshold based on the input supply voltage.

 

 Figure 1. SIMPLE SWITCHER® LM43602 Enable

Figure 1. SIMPLE SWITCHER® LM43602 Enable

 

However, not all regulators have a precision enable function. For converters with logic level EN input, a simple external UVLO circuit can be used to generate the EN signal based on the required VIN range of the converter. The external UVLO circuit provides a logic low signal that keeps the converter disabled until the proper input voltage is reached. 

 

Two simple UVLO schematics can be seen in Figures 2 and 5. The UVLOs were hooked up to the LM22672 step-down converter which was set to produce an output voltage of 5V. The first schematic uses two NPN transistors. Figure 2 shows two potentiometers, RT and RH, used to adjust the UVLO turn-on voltage as well as the hysteresis respectively.

 

Figure 2. Simple UVLO Circuit #1

Figure 2. Simple UVLO Circuit #1

Figure 3 shows the VIN, VEN, and VOUT waveforms of the UVLO and converter from Figure 2.

 

Figure 3. UVLO Controlled Waveforms

Figure 3. UVLO Controlled Waveforms

The EN voltage comes up when VIN has reached the operating range of the design. The output of the converter is able to produce a consistent 5V when the enable pin is logic high. 

 

It is always a good idea to have some hysteresis on the turn-on threshold. The hysteresis in this case is set by RH. Figure 4 shows what happens when there is no hysteresis on the UVLO threshold. As the input voltage is hovering around the threshold, the VEN pin can be seen chattering on and off at a high frequency. The enable pin is turning on and off too fast for the converter to start up at all.

 

Figure 4. UVLO without Hysteresis

Figure 4. UVLO without Hysteresis

 

The second external UVLO circuit uses an NPN and a PNP transistor. In Figure 5, potentiometer RB allows the user to set the VIN UVLO threshold while potentiometer RH sets the hysteresis value.

 

Figure 5. Simple UVLO Circuit #2

Figure 5. Simple UVLO Circuit #2

 

Figure 6 shows the UVLO successfully enabling and disabling the step-down converter at the set VIN thresholds.

 

Figure 6. UVLO Controlled Waveforms

Figure 6. UVLO Controlled Waveforms

So, if you find yourself with a converter requiring a logic level enable input and you need a more precise UVLO, take one of the circuits above and adjust the two resistors to set the enable threshold and hysteresis as desired. Simply hook the output of the UVLO circuit up to your IC’s enable pin and you’re good to go!

 

What's your favorite UVLO circuit?  Please feel free to comment below.

 

Additional resources:

Anonymous
  • Nadav

    The value of the Zener should be chosen close to the point you wish the UVLO to trip.

    Resistor RT is used to adjust the trip point; I would start with a 10K or so.

    Resistor RH is used to adjust the hysteresis of the trip point; I would use a 100K or 1Meg to start with.

    This circuit is experimental, so feel free to adjust the component values until you arrive at a response that

    works for you.

  • Hi,

    Thanks for a great post!

    I'd like to build and test the uvlo circuits suggested above, however, some of the parts in the schematics don't have values, namely: RH, RT & the Zener diode.

    Could you please clarify what are the values of these parts?

    Also, how precise do the resistors in the circuits need to be (1%, 5%, etc.)?

    Many thanks in advance.