A DC/DC converter with low efficiency and excessive component-temperature rise can be a major headache – even more so if you must redesign the circuit or revise the board layout.
To avoid such headaches, it seems prudent to have an in-depth understanding of a converter’s operating modes and power losses. And while easy-to-use converter design and simulation tools offer a quick way to choose components, plot efficiency curves, and estimate power losses within the converter, the nuances of a particular power stage and its various operating modes often remain misunderstood. Identifying the converter’s modes and dissecting the expressions required to predict power losses can give you a full appreciation for a DC/DC converter’s electrical and thermal behaviors.
Figure 1: Four-switch synchronous buck-boost converter schematic with a peak/valley current-mode controller. The power-stage high-current connections are denoted in red.
Power-stage operating modes
Figure 1 is a schematic of a four-switch buck-boost DC/DC converter with a 4.5V-42V input range and a 12V output. As mentioned in this video demonstration, this converter has three specific modes of operation depending on input voltage relative to the regulated output voltage set point:
-
Buck mode with VIN > VOUT.
-
Boost mode with VIN < VOUT.
-
Buck-boost transition mode with VIN close to VOUT.
Using an equivalent circuit to model the power stage as a cascaded connection of buck and boost stages, you can find the relevant duty cycle for each metal-oxide semiconductor field-effect transistor (MOSFET) depending on the mode of operation. This is the first step to deriving efficiency and power losses over input-voltage and output-current ranges.
A recent article that I wrote for How2Power.com titled “Optimizing the Efficiency of the Four-Switch Buck-Boost Converter” analyzes each mode of the circuit shown in Figure 1, providing expressions in tabular format to quickly capture and validate power-stage losses. In fact, because the analysis I described in that article leverages two fundamental and easily understood topologies (buck and boost), it is generally applicable to almost any DC/DC converter, including TI Fly-Buck™ converters, forward and full bridge.
Converter power losses
I identified the most notable component power losses in the How2Power article and will summarize them here. I aggregated the losses to gauge their impact on converter efficiency; see Figure 2.
- Power MOSFET losses:
- Conduction loss related to RDS(on).
- Switching loss, including body-diode reverse recovery
- Dead-time loss from body-diode conduction.
-
Inductor copper and core losses.
-
Shunt resistor loss.
-
Gate driver loss.
-
Pulse-width modulation (PWM) controller bias-supply and quiescent loss.
Figure 2: Four-switch buck-boost converter efficiency and component power-loss breakdown versus input voltage, VOUT = 12V.
Having an instinctual understanding of these losses – particularly for high-density designs where size reduction is essential – not only helps when selecting components, but also paves the way for optimal thermal design and printed circuit board (PCB) layout. I measured the plot in Figure 2 using a 400kHz four-switch buck-boost converter design supplying a 12V, 6A load. The design achieves greater than 95% efficiency across a 6:1 input-voltage range. Peak efficiency is reached when VIN equals VOUT in buck-boost transition mode.
Clearly, then, in the push for smaller-footprint DC/DC converter solutions, you can succeed in uniting two characteristics that are normally mutually exclusive: lower component temperatures and higher usable power.
Additional resources
-
Review the design equations for a four-switch synchronous buck-boost converter.
-
Take a look at the high-density evaluation module (EVM) for the LM5175 buck-boost controller.
-
Understand the efficiency/size trade-off dilemma amid the push for smaller-footprint solutions.
-
Read this TI E2E™ Community blog post on the “Five stages of system and thermal component design.”
-
Check out detailed application notes on thermal design.
-
Start a design now with WEBENCH® Power Designer.