Minimize the impact of the MLCC shortage using D-CAP+™ control mode

As my colleague Yann said in an earlier technical article, there is a growing shortage of multilayer ceramic capacitors (MLCCs), and the situation is likely to persist through 2020. MLCCs are used in almost every type of electronic equipment, due to their reliability and small footprint.

Manufacturers are now looking to replace ceramic capacitors with polymer or other capacitor types. TI D-CAP+™ control mode multiphase controllers, converters and modules (like the TPSM831D31) can help hardware designers reduce the MLCC count on their motherboard versus competitive solutions.

D-CAP+ control mode is a TI proprietary pulse-width modulation controller and converter control architecture that enables very easy loop compensation and excellent loop stability in the presence of varying conditions such as input voltage and the number of phases.

It is a current-mode constant on-time control that uses a true inductor current-sense implementation rather than the injected or emulated ripple current schemes used in the D-CAP2™ and D-CAP3™ control topologies. The D-CAP+ control mode has fixed on-time in steady state and adaptive off-time during load transient conditions (AC response), in which the off time is adjusted and more pulses are generated (pulled in) to respond quickly to load transients and maintain the output voltage in regulation. 

Since the on-time is regulated, there’s a natural period stretching in discontinuous conduction mode (DCM), producing higher efficiency and smooth control when crossing the continuous conduction mode and DCM boundary. D-CAP+ control mode is extremely easy to compensate and does not require the complex type-3 compensation circuits required in voltage-mode control architectures. For more information on D-CAP+ control mode, see the 2014 Power Supply Design Seminar paper, “Choosing the Right Variable Frequency Bulk Regulator Control Strategy

Because D-CAP+ control mode can respond much faster to a processor/application-specific integrated circuit/field-programmable gate array load transient than a fixed-frequency control architecture, it can meet tight tolerance specifications without the number of MLCCs that you would otherwise need for discharging or charging to provide the required energy to the load.

Figure 1 compares a TI voltage-mode controller vs. a D-CAP+ controller during such a load transient. The TPS53647 D-CAP+ control-mode controller has lower overshoot and undershoot, despite having a lower crossover frequency.

Figure 1: Load transient response comparison between voltage-mode and D-CAP+ controllers

The results are similar when making comparisons to competing multiphase controllers with non-D-CAP+ control. Figure 2 compares a 60-A load step from 180 A to 240 A at a 1-kHz load transient repetition rate. The D-CAP+ controller, again, results in lower overshoot and undershoot. These results were replicated on the same motherboard under the exact same conditions. The TPS53681 D-CAP+ controller can achieve better load transient response and faster output voltage settling.

Figure 2: Load transient response comparison between a competing device and TI’s D-CAP+ controller

As a final example, let’s compare a central processing unit (CPU) vendor’s reference design to our own Vcore design. The thermal design current (TDC) was 116 A, while the maximum current (IMAX) was 395 A.

The test data shows that the D-CAP+ controller enables a faster load transient response, which translates to significant MLCC savings vs. the CPU vendor reference design.

Table 1 summarizes the results. The D-CAP+ control solution still meets the CPU overshoot and undershoot specifications while eliminating 42 MLCCs and >700 µF of output capacitance. The Table 1 comparison is applicable to any D-CAP+ control-mode voltage regulator vs. competing regulators.

 

Table 1: CPU reference design vs. D-CAP+ solution MLCC count comparison for a 116-A TDC and 395 IMAX design

MLCC shortages are not going away anytime soon. If you want to reduce the MLCC count in your design bill of materials so that you can get new projects to market faster, consider using TI’s D-CAP+ controllers, converters and modules.

Additional resources

Anonymous
  • Thank you George, it really helps a lot. I have questions.

    1. From table 1, what type of bulk capacitor is used? Does the type of capacitor make difference on the transient performance?

    2. You said that MLCC is replaced with Polymer or other types of capacitor. Can I find any articles covering the effect of replacing MLCC with Polymer in terms of feedback loop, such as an effect of higher DCR?