Alex Triano
Designers will often use a transient voltage suppression (TVS) diode to clamp large surge currents to a safe voltage level in order to protect nearby components from damage. In many ways, a TVS diode behaves like a Zener diode, but with a higher power-rating capability because of its larger die size and stronger wire bonding.
In a hot-swap application, if there is a large overcurrent fault, then the protection integrated circuit (IC) will shut off the current quickly in order to shield nearby components from damage. This fast shutdown of current – from maybe 50 A (overcurrent) to 0 A (shutoff for protection) – can occur within tens of nanoseconds and results in a large current transient (di/dt), as shown in Equation 1:
This current will be trapped as energy inside of trace or wire inductance on the input. Although the trace inductance may be low, at a value of about 10 nH, it will still produce a surge on the input of the hot-swap controller, based on Equation 2:
That -50-V surge will be in series with the input power supply and will effectively create a positive voltage spike on the input rail, often exceeding the voltage rating of the hot-swap controller IC or metal-oxide semiconductor field-effect transistor (MOSFET) drain-to-source voltage (VDS) (see Figure 1). To prevent this voltage surge from occurring, you can place a TVS on the input to divert energy from the inductance straight to ground. The optimal placement of the TVS will be after any series inductance on the input (such as after a fuse).
The simplest way to pick a TVS diode for a hot-swap application is to choose one that meets the following three criteria:
For a 12-V high-power application, a common TVS choice is the 5.0SMDJ12A, which has a 5-kW transient power capability. For a deeper analysis of the equations used in choosing a TVS diode for a hot-swap application, check out the Power Electronics article, “TVS Clamping in Hot-Swap Circuits.”
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated