Low Power Orientation Tracker Enabled by IQmathLib

Have you ever worried about your packages being mishandled during shipment? Have you ever been concerned about potential theft of your valuable assets? Have you ever gotten lost, while searching for a room in a large building? Are you shying away from addressing these questions due to cost or power limitations?

Maybe all you need is an MSP430 MCU running a Low Power Orientation Tracker. By combining the MSP430 G2 LaunchPad with CircuitCo's Educational BoosterPack, enables the MSP430 MCU to interface with an accelerometer for regular sampling that can be interpreted as x, y, and z coordinates of gravity. Arc Tangent can then be used to calculate current orientation, including angles for pitch and roll. To cut the cord and switch over to battery operation, the Fuel Tank BoosterPack can be plugged in to the design. If you need to track assets from a central location, a number of wireless BoosterPacks are also available for the LaunchPad ecosystem. The best part is that all of these components are online and you can even build your own variant by using the open source design files.

Using the hardware described above, you could create a low-cost design that can be used to track orientation change across shipments, or in warehouse environments to ensure products are handles properly and only when needed. By excluding additional hardware, such as a gyroscope and using optimized software, this design can remain in low-power modes for the majority of the time. This means potential applications such as indoor navigation are also possible.

 

Now, you may be asking yourself, how easy is it to do complex math on an MSP430 and maintain ultra-low power consumption? The answer is it has never been easier!

IQmathLib is a library of optimized fixed point math functions, now available for MSP430 MCUs! Not only is this library free, but it is available standalone or integrated in Code Composer Studio. With this library in hand, all you need to worry about is the application. No need to spend months optimizing fixed point functions on your own! If you want the data flexibility of floating point, MSPMATHLIB is available as well, but if getting the best performance and/or the lowest power consumption out of your MSP430 MCU is top priority, this is the library for you! With IQmathLib, you could get more than 100x better performance running common math functions.

So now is the time to seize the day! Say NO, to damaged packages, stolen items, getting lost finding your colleagues at work, and more. Checkout the Low Power Orientation Tracker today and get to work with the IQmathLib software library that enables it to be lower-power than ever before.

Do you have other plans for IQmathLib? Leave a comment and let us know!

Anonymous
Parents
  • Add a decent LCD screen, a keypad, a battery and a case - you have a custom scientific calculator.  With the added benefit of being able to collect data from assorted transducers.

    Competitors include the WP-43S, the enthusiast's calculator, still in development over at HP Calculator Museum...

Comment
  • Add a decent LCD screen, a keypad, a battery and a case - you have a custom scientific calculator.  With the added benefit of being able to collect data from assorted transducers.

    Competitors include the WP-43S, the enthusiast's calculator, still in development over at HP Calculator Museum...

Children
No Data