I came across a really odd issue while  I was debugging the LMP91300.You see,when I use the LMP 91300 with a resonant circuit that has a 47uH inductor and a 1.5nF capacitor,it just stays lit up all the time after I power it on.But if I switch to a resonant circuit with a 36μH inductor and a 1.8nF capacitor,it works perfectly fine.I have ruled out the issue with the register setting.What could possibly be causing this?