///////////////////////////////////////////////////////////////////////////////////////
//
//	EVF_Workbench Setup Readme.txt
//
//	$Source: /home/cvs/EVF_Workbench/EVF_Workbench/readme.txt,v $
//	$Revision: 1.4 $
//	$Date: 2009/11/20 19:42:57 $
//	$Author: jonesj $
//
//
///////////////////////////////////////////////////////////////////////////////////////

//////////////////////////////////////////////////////////////////////////////////////
//
//  EVF_Workbench license notice
//
//////////////////////////////////////////////////////////////////////////////////////

C) Copyright National Semiconductor Corporation 2009

                All rights reserved

National Semiconductor Corporation (hereinafter referred 
to as "National") hereby grants the user of EVF_Workbench 
(hereinafter referred to as "this software") a non-exclusive, 
nontransferable license to use this software under the 
following terms.  Before using this software, the user 
should read this license.  If the user does not accept 
these terms, the software should be returned to National 
within 30 days.

This software was developed using the wxWidgets 
library and, as such, it is subject to the provisions
of the wxWidgets Library License.  A copy of this license
is contained in the accompanying license.txt file.

The user is granted this license only to use the
software and is not granted rights to sell, load, rent,
lease or license the binary distribution of this software 
in whole or in part, or in modified form, to anyone else.

This software is provided on an "AS IS" basis and 
National makes absolutely no warranty with respect to the 
information contained herein. NATIONAL DISCLAIMS AND CUSTOMER 
WAIVES ALL WARRANTIES, EXPRESS OR IMPLIED, INCLUDING 
WARRANTIES OF MERCHANTABILITY OR FITNESS FOR A PARTICULAR 
PURPOSE. The entire risk as to quality and performance is 
with the Customer. ACCORDINGLY, IN NO EVENT SHALL THE 
COMPANY BE LIABLE FOR ANY DAMAGES, WHETHER IN CONTRACT OR 
TORT,INCLUDING ANY LOST PROFITS OR OTHER INCIDENTAL,
CONSEQUENTIAL, EXEMPLARY, OR PUNITIVE DAMAGES ARISING OUT 
OF THE USE OR APPLICATION OF THIS SOFTWARE.  Further, 
National reserves the right to make changes without notice 
to this software to improve reliability, function, or design. 
National does not convey any license under patent 
rights or any other intellectual property rights, including 
those of third parties.

National is not obligated to provide maintenance or support 
for this software.

National may provide, at its option, the source
code for this software.  If this source code is provided, it
is provided under the provisions of the GNU General Public
License, version 3, contained in the accompanying license.txt 
file.  National is not obligated to provide source code.

/////////////////////////////////////////////////////////////////////////////////
//
//  Welcome to EVF_Workbench setup!
//
/////////////////////////////////////////////////////////////////////////////////

This installer will install EVF_Workbench on your computer.  EVF_Workbench is a graphical
front-end for National Semiconductor's svf2evf.exe conversion program.

To perform the installation:

1) Save the .zip file containing this readme file to a convenient location on your computer.
   Common locations include the desktop,  "My Documents", or c:\temp, the temporary files 
   directory.
2) Extract all the files in the .zip archive to a convenient folder on your computer where you
   can find them again.  The destination for the files need not be empty, but if it already
   contains a file with a name the same as one in the .zip file, you will be prompted to overwrite it.
3) Locate the setup.exe icon in the folder where you unzipped the installation files and 
   double-click on it to run it.  You can also run it from a command-line window if you prefer,
   or by using the "Run..." icon in your start menu.  Make sure you execute the correct setup.exe
   because many installation programs share this executable name.
4) Follow the installation instructions to install the program to the desired location.

Installation notes:

EVF_Workbench setup will install the EVF_Workbench executable by default to the following folder,
creating it if it does not already exist.

C:\Program Files\National Semiconductor Corp\EVF_Workbench

The setup program will also create four subdirectories of the installation directory:

.\ConfigFiles
.\SVF_Demo_Files
.\EVF_Demo_Files
.\EVF_Workbench_Help

These directories contain the required configuration files for the svf2evf conversion program,
some sample SVF files that can be used to test the operation of the EVF_Workbench program, 
some sample EVF files created using the program, and a compiled HTML help file to be used 
with Microsoft Windows(R) help.

Setup will also install the current version svf2evf.exe console application, which can be 
run stand-alone from a command-line window if desired.  This console application must reside
in the same directory as the EVF_Workbench executable.  If it does not, EVF_Workbench will
not run properly and will report an error.

Setup will also install a default svf2evf conversion script default.ecs.  This script 
specifies the default install directories, so it will not run without modification if the 
program is installed somewhere other than the default.  The script is a simple ASCII file,
however, and can be easily modified with any available text editor, such as notepad.

Setup will (optionally) create shortcuts to EVF_Workbench on your desktop and in your 
Start menu.  In the Start menu, the shortcut will appear in a program group called
National Semiconductor Corp.

Once you have run the setup.exe program, it is okay to delete all the files extracted from
the .zip file as well as the .zip file itself.  If you think you might want to reinstall the
program later, just save the .zip file and follow the above instructions again.

This readme file and the license.txt file will be copied to the directory where the program 
is installed if you need to refer to them again.